5G NR
These editing functions are available for downlink and uplink BWPs and the following channel types: DCI, DL-SCH, CSI-RS, PRS, UCI, UL-SCH, and SRS.
Tap or click the plus sign (+) to add a BWP or channel to the bottom of the edit list. The new entry also appears in the corresponding summary table below, showing its parameters. Use the edit menu (...) to delete or copy the currently selected item in the edit list. The summary table updates accordingly. (View
Figure 1.) Each new entry is given an auto-filled descriptive name. BWP names are read-only. Channel names can be edited.
Whenever you delete a BWP or channel, a re-indexing (
Figure 2) of the remaining BWPs or channels occurs, updating the ID numbers. An index/cardinality of a BWP or channel starts from 0, with a valid index or cardinality range from 0 to the channel count, or BWP count minus 1.
Do not try to access BWPs or channels that do not exist.